Advanced Video Analytics and Security

    Protection of mission critical assets, both from security surveillance and operational monitoring perspectives.

Default Alternative Text

Challenges

Not having the ability to monitor critical parameters, internally and externally, at all times, has been an ongoing challenge within the industry. Schneider offers robust 24/7/365 day solutions for surveillance and operational monitoring that address safety, regulatory and preventative maintenance needs for all types of facilities.
  • Value Proposition

    Schneider Electric's robust thermal and thermography solutions allow for:

    • Integration into various backend systems (VMS, SCADA, HMI, PLC).
    • Protection of mission critical assets from both security surveillance and operational monitoring perspectives.
    • Advanced analytic engine of sending data that can be utilized for trending analysis of key data points, as well as alarms for both parameter and equipment breaches.
    • The ability to send data and/or video to the headend systems, allowing for coverage in low bandwidth situations.
  • Differentiation

    Schneider Electric's infrared thermal and thermography solutions are the only ones that allow for:

    • Third-party integration.
    • Advanced video analytics, that do not require a license fee.
    • Ability to stream data, and video with embedded data.

The Chat is available now