• Keeping the power on: How to manage backup battery systems

Default Alternative Text
Preventable issues and manufacturing errors combine for a total of 69% of battery failures. Source: Report of the Battery Council International, 2010.

Emergency power systems rely on batteries to deliver power at the right moment to start a generator or to run a UPS. Neglected batteries, however, are the most common reason for backup power failure, which is why facility managers use automated battery testing systems to assess battery health.

Issues that can affect battery performance include:

  • Batteries don’t display outward indications of impending failure.
  • Replacing batteries before end of life can invite new risks of manufacturing errors.
  • Depending on usage, a battery may fall short of lifespan expectations.
  • High temperatures within battery cells can accelerate corrosion.
  • Undercharging can lead to capacity loss; overcharging can cause cells to dry out.

Analysis of battery health should be an expected part of any effective healthcare or critical power facility design and energy management plan for uninterrupted power – and peace of mind.

Discover how to ensure your battery backup system can do its job in protecting critical facilities from power failure.
Learn more

The Chat is available now