• Getting schooled in energy efficiency

Sustainability consulting between two construction workers, energy efficiency, water management.

Experts estimate that over 41% of Fortune 500 companies now use education technology to train employees. Replacing classroom learning with online options delivers measurable outcomes, including the following four business benefits:

  • Lower operating expenses
  • Improved productivity 
  • Increased retention of course material 
  • Reduced environmental impact

E-learning courses consume 90% less energy than traditional courses and result in 85% lower CO2 emissions per student. It also eliminates time spent travelling to offsite facilities and minimizes lost work time.

Discover the benefits of online learningDiscover the benefits of online learning
Learn more

The Chat is available now