• Five reasons why aluminum piping makes sense for compressed air systems

Default Alternative Text

Aluminum piping offers many advantages for compressed air installation including reduced costs and increased longevity. Courtesy: TransairTraditionally, engineers have specified a variety of piping materials for compressed air systems, including black iron, galvanized steel, copper, stainless steel and even plastic. More recently, aluminum piping has become an option considered by many contractors, architects and engineering firms. Aluminum piping makes sense for compressed air systems in many different applications.

Black iron and galvanized steel pipe are two common types of pipe used for compressed air systems. More than 60% to 70% of all compressed air systems installed today use black iron or galvanized pipe, due to a variety of factors:

  • Contractors are familiar with these materials.
  • Material costs are low.
  • The pipe and compressed air system fittings are readily available.
  • Steel pipe is rated for high pressure.

There are, however, five key reasons why aluminum piping is a superior material to use for most compressed air installations today, each of which addresses a key disadvantage to traditional pipe systems.

1. Lowering Installation Costs

Table 1: Compressed Air Pipe Material Selection – Advantages and Disadvantages Comparison (for further comparison information go to Opus.mcerf.org). Courtesy: TransairMore time is needed to install a compressed air system when using steel pipe compared to installing a system using other materials.

One factor behind this is that steel pipe must be threaded in order to join pipes and install the proper fittings. To properly thread steel pipe, you need special threading equipment and skilled workers to operate it. These workers cost more than unskilled workers, and that also drives up installation costs.

Also remember that threading pipes is dirty work. You need cutting fluids to get a good thread, and that must be cleaned from the pipe before you can start using the system. Threading also creates a lot of debris.

Modifying and maintaining a compressed air system made with steel pipe is more difficult than modifying and maintaining systems built from other materials. One reason for this is that steel pipe is much heavier than other materials. Because steel pipe is so heavy, it requires more labor (read as higher labor costs) to handle the piping while making modifications than it would to make modifications to a system made with other piping materials.

2. Minimizing System Leaks

Another issue with threaded connections is that they will inevitably leak. It’s been estimated that eight to 10% of the compressed air in a system will leak through threaded connections. This causes compressors to run harder and longer, driving up utility costs.

3. Aluminum Piping Doesn’t Corrode

A common problem with using steel pipe is that moisture inside the system will cause pipes to rust from the inside out. Even if your compressed air system has a moisture trap, there will be some moisture in the system and corrosion will occur. Even galvanized steel pipe will corrode, as not all pipes are galvanized both inside and out.

Asset validation and optimization

Asset validation and optimization is a process that requires the involvement of subject matter experts (SMEs), process engineers, reliability engineers, planners, the maintenance department, instrumentation SMEs, and electrical SMEs, to name a few. 

This makes the air compressor work harder to maintain the pressure of the system. In extreme cases, loose scale can completely clog a line or damage equipment connected to a line. Of course, corrosion and loose scale affects air quality and makes it unsuitable for applications that require clean air.

4. Aluminum outperforms the copper alternative

Copper piping is another solution for compressed air systems and is attractive because it doesn’t corrode as much as steel pipe. While it can corrode, it doesn’t have pipe scaling like steel pipe. This means that a copper system will have fewer air flow problems and air cleanliness problems than steel pipe, but it can still experience flow restriction over time.

A copper solution comes with its own set of disadvantages, however; perhaps the biggest is the cost of copper material itself. In October 2011, the price of copper increased by 20%, and subsequently, so did the price of copper pipe. Even though prices have dropped since then, the fact remains that copper pipe continues to be considerably more expensive than steel pipe.

Another disadvantage is that fittings must be soldered, and this causes its own set of problems. Soldering of course requires an open flame, making this a safety issue in some environments. And, soldering requires some skill to accomplish, an increasing problem in an era when skilled labor is becoming harder to find. If a joint is not soldered properly, it will leak, and leaks increase energy costs.

Finally, not all types of copper piping are suitable for use with high air pressures. So, if you’re planning to use copper, you have to make sure that you choose a pipe that can handle the pressure.

5. PVC and stainless steel present obstacles in cost and durability

While steel pipe and copper pipe are the two most widely used materials for compressed air systems, you will also sometimes find systems that use PVC pipe and stainless steel pipe. In fact, it is against OSHA standards and highly dangerous to use PVC pipe for compressed air systems. PVC becomes brittle over time and may explode when transporting air under high pressure.

Stainless steel is another option, especially when the compressed air system is to be installed in a corrosive environment. In some cases, stainless steel is considered an option depending on the fluctuating cost of copper pipe.

As with other steel pipe systems, though, stainless steel systems can be costly to install. Threaded stainless steel pipe can be difficult to seal, often requiring the use of lubricants to thread correctly. Welding stainless steel drives up installation costs and safety concerns through the need of a skilled welder, and the added risk of smoke inhalation, damage to eye sight, and fire.

The case for aluminum piping

In recent years, aluminum piping has become a solid alternative to other piping materials for compressed air systems. Compared to the materials described above, installing a compressed air system using aluminum piping offers many advantages:

  • Aluminum pipe systems are much easier to install and to modify than steel or copper pipe systems. Labor savings of 50% can be achieved, since aluminum pipe is supplied ready for use. No particular preparations beyond cutting, deburring, and chamfering are required, nor are special tools needed. Aluminum pipe is calibrated, meaning that its diameter is strictly controlled. This means that associated quick connect components will fit securely, and each connection is automatically secured.
  • Aluminum pipe is much lighter than steel pipe or copper pipe. This also reduces installation and modification costs.
  • Another factor that makes aluminum pipe systems easier to install and modify is that it doesn’t require threading or soldering.
  • The compressed air provided by a system built with aluminum piping is much cleaner than air delivered by a steel pipe system. Aluminum pipe systems can help meet the requirements of ISO 8573-1: 2010 air quality standards, should the application require it. Cleaner air also means lower maintenance costs.
  • Aluminum pipe’s corrosion-resistant properties mean optimal air flow, reduced energy costs, and better air quality.
  • The fittings used with aluminum pipe systems fit securely and leak far less than the fittings used with threaded systems. This translates directly into energy savings and improved plant productivity.

Naturally, there are some disadvantages. For example, material costs are higher for aluminum pipe systems compared to steel pipe systems. When compared to copper pipe systems, however, material costs for aluminum are about the same or even lower. And, the working pressure for aluminum is 232 PSI at 115 degrees. Overall, though, for many applications, aluminum piping is a solid alternative for compressed air systems.

Kyri McDonough is Transair marketing services coordinator.

PLEx_Logo_Color_TM
Powered by ContentStream®

The Chat is available now