Technical FAQs

Ask a Question

Filter results

Clear
Preventa XY2C - Dimensions of the XY2CZ901 bellow for XY2CE rope pull switch
Find attached dimensions of the XY2CZ901 bellow for XY2CE rope pull switch. Attachment shows image of this XY2C accessory and gives material.
How can I distinguish thermal from magnetic faults when using GV2ME, GV2P, GV2L and GV2LE?
Using a GVAM11 combined with a GVAD10xx, it is possible to distinguish between thermal and and magnetic faults.   If there is no fault:  GVAM11: contact...
Does Schneider Electric offer a direct replacement for Lexium Integrated Drive type ILS1B853S1460 ?
Check the motor label and verify the ID number of 66109300010 is found on the label. If the ID number is 66109300010 the the exact replacement for...
What causes "dis" error on Lexium 32 ?
The error "dis" seen on the display of Lexium 32 is caused by the following possible faults. 1. Missing mains voltage.   ( missing mains voltage will...
What is the heat loss of the GV2 P / ME /RT thermal magnetic circuit-breakers?
The heat dissipation of GV2P/ME/RT circuit breakers is 2.5 W per pole, i.e. 7.5 W in total.
What should I do if I lose my password on an XBTVA?
If a password is lost on an XBTVA, place a male connector in the XBT's serial link connector. On this male connector, create a link between the following...
When should the protective film on my HMI be changed?
A screen protector which has been used for a long period of time may have scratches or dirt on it, and could have lost much of its water resistance....
What is the part number for the main control board for the ATS46?
Issue: What is the part number for the main control board for the ATS46? Product Line: Altistart ATS46 Environment: All Cause: Replacement part Resolution:...
What are the part numbers for the Gate Driver Boards for ATV66 drives?
Issue: What are the part numbers for the Gate Driver Boards for ATV66 drives? Product Line: ATV66 Drives Environment: Gate Driver Boards Resolution:...
Can I purchase touch-up paint for KQII distribution boards and I-Line panelboards?
Yes, our product code is SDPAINT.  Please contact our Customer Interaction Centre for price and availability or to place an order. Tel 0870 608 8 608
Results 51 - 60 of 86