Technical FAQs

Ask a Question

Filter results

Clear
What is the Schneider Electric replacement for the Berger Lahr VRDM3913/50 LNB motor with ID number 5212701600
The replacement for the VRDM3913/50 LNB motor with ID number 52127016000 is now Schneider Electric part number BRS39BN760ABA This is considered a...
Does Schneider Electric offer a replacement for the Berger Lahr WPM-311 controller?
The entire product line of WPM-311 type controllers from Berger Lahr are obsolete and no longer available Schneider Electric does not offer a drop...
Does Schneider offer a replacement for the Berger Lahr D065 Icla motor with ID number 59600100028?
The replacement model for replacing D065 with ID number 59600100028 is the model  N065 of the Icla product line. The ordering number from Schneider...
What is the pin assignment of the RS485 modbus connection on the Schneider Electric adapter TCSMCNAM3M002P ?
Pin 4 of the RJ45 connector is MOD_D1 Pin 5 of the RJ45 connector is MOD_D0 Attached you will also find the pin assignment of the RJ45 ModBus connection...
Does Schneider Electric offer the servo motor type BMH1002S0015 ?
No, the BMH1002S0015 is a special version for the company W & H and is a proprietary product which is not available directly from Schneider Electric....
Does Schneider Electric offer a direct replacement for the Berger Lahr D900 series of drive cards?
No, there is no drop-in replacement available to replace the Berger Lahr D900.xx drive cards. This includes all versions of D900.   D900.00, D900.50,...
How do I de-mount the circuit breaker in GenieEvo
The GenieEvo circuit breaker can be de-mounted and replaced in under 1.5 hours. Full details of how to de-mount the breaker are on the attached procedure....
Can the displays for the PM700 and PM800 range of panel mounted power meters be purchased separately
No, the displays for the PM700 and PM800 range of panel mounted power meters are not available separately.
Does Schneider Electric offer the Lexium Integrated Drive model ILS1R573S1341 ?
No, ILS1R573S1341 is not available for purchase from Schneider Electric. ILS1R573S1341 is an OEM specific model which s proprietary for the OEM and...
Can I use the 63A 3P busbars of the GV2 range on the Tesys U range?
The 63 A 3-pole busbars are identical for pre-wiring several modules of the following type: GV2 circuit breakers LC1D contactor TESYS U starter-controller...
Results 41 - 50 of 86