Technical FAQs

Ask a Question

Filter results

Clear
Does Schneider Electric offer a replacement for the Berger Lahr WPM-311 controller?
The entire product line of WPM-311 type controllers from Berger Lahr are obsolete and no longer available Schneider Electric does not offer a direct...
How can one troubleshoot a S-Flex drive if it will not run in AFC or Bypass?
Issue: How can one troubleshoot a S-Flex drive if it will not run in AFC or Bypass? Product line: SFD212, S-Flex Environment: All models with Bypass...
Can the displays for the PM700 and PM800 range of panel mounted power meters be purchased separately?
No, the displays for the PM700 and PM800 range of panel mounted power meters are not available separately.  There is a remote display unit for the...
Why does the PM750MG meter display incorrect power readings or not show any current?
The connections from S1 and S2 on the current tansformer to I+, and I- on the back of the meter might be reversed, ensure that the wiring of the meter...
What are the part numbers of the replacement contact sets for LC1F power contactors?
Spare parts required for each pole of LC1Fxx contactors are as follows:   2 fixed contacts 1 moving contact 2 deflectors 1 backplate Locking screws...
Can I replace the backlight in an XBTGT HMI?
It is possible for a customer to replace the backlight in certain HMIs, but not all of them. The XBTGT5000/6000 and 7000 series HMI backlights can...
Can the displays for the PM700 and PM800 range of panel mounted power meters be purchased separately?
No, the displays for the PM700 and PM800 range of panel mounted power meters are not available separately.  The PM700 and PM800 are now obsolete There...
I require spares for FBX100 floor box are they still available?
Below are the spares for the FBX65, FBX75, FBX100, FBX 120 old floor boxes, parts may be limited due to product being obsolete : 600055 M4 x 8 POZIPAN...
I have a LexCom Home System and I would like a spare part
LexCom Home is no longer distributed by Schneider Electric. For you spare parts requirements please contact: Western Electrical Cofton Road Marsh...
What is the replacement power board part numbers for the Altivar ATV58 drives?
Issue: What is the replacement power board part numbers for the Altivar ATV58 drives? Product Line: Altivar ATV58 or Flex58 Environment: All Cause:...
Results 21 - 30 of 86