Technical FAQs

Ask a Question

Filter results

Clear
Is it possible to copy the program out of an LMC20 motion controller?
Yes, it is possible to copy the program out of an LMC20 motion controller. There can be instances in which an LMC20 needs to be replaced and the program...
Are spare part available for the MGFA Switch Disconnector Fuses and the MGFL Switch Disconnectors?
The only parts that can be replaced are the fuse links in the switch disconnector fuses. Please see attachment for details of the fuse links.
Are spare parts available for the MGFS Fuse Switch Disconnectors and MGFD Switch Disconnectors?
The only parts that can be replaced are the fuse links in the fuse switch disconnectors and the solid copper links in the switch disconnectors. Please...
What is the repair process for contactors?
The LC1K, LC1D and LC1F families of contactors cannot be repaired, as the cost of repairing any of these contactors is generally higher than its manufacturing...
What product replaces Lexium 15 or Lexium 17 drives
The migration path for replacing obsolete Lexium 15 or Lexium 17 drives is the Schneider Electric Lexium 32 product line. However, in order to make...
Does Schneider Electric offer spare boards for Berger Lahr SST control systems.
No, the SST control systems are no longer supported and there are no spare parts offered by Schneider Electric to support these products. All boards...
Does Schneider Electric offer motor type BRX184 found on a W&H printing press?
The BRX184 motor type is a special customized product for the company W&H  (Windmoeller & Hoelscher) Because this is a customized product it is not...
Does Schneider Electric offer a replacement for the Berger Lahr WPM-311 controller?
The entire product line of WPM-311 type controllers from Berger Lahr are obsolete and no longer available Schneider Electric does not offer a direct...
How can one troubleshoot a S-Flex drive if it will not run in AFC or Bypass?
Issue: How can one troubleshoot a S-Flex drive if it will not run in AFC or Bypass? Product line: SFD212, S-Flex Environment: All models with Bypass...
Can the displays for the PM700 and PM800 range of panel mounted power meters be purchased separately?
No, the displays for the PM700 and PM800 range of panel mounted power meters are not available separately.  There is a remote display unit for the...
Results 11 - 20 of 87