Technical FAQs

Ask a Question

What is the replacement for the XBTGT7340?
Issue: What is the replacement for the XBTGT7340? Product Line: Magelis HMI, XBTGT7000 series Resolution: The replacement for the XBTGT7340 is the:...
Can I use the PCFL_AIN block with M340 analog IO?
Yes, you can use the PCFL_AIN block with M340 analog IO. However, you will experience better resolution and scaling capability by using the BMXAMx...
Connect and change parameters on a LXM32 drive using SoMachine
Issue: Can I connect and change parameters on LXM32 servo drive using SoMachine? Product Line: SoMachine Resolution: In SoMachine, when you add a...
Why am I having issues connecting SoMove to an Altivar Drive or Altistart Soft Starter?
Issue: SoMove Troubleshooting:Cannot Connect to SoMove using an Altivar Drive  Product Line: Altivar Drive (ATV61, ATV71) Altivar Machine Drive (ATV12,...
Can I convert an XBTL1000 application (XBTF terminal) to Vijeo Designer (XBTGT/GK terminal)?
We have a Services & Projects offer making it easy to migrate XBTL 1000 applications created on XBTF terminals to Vijeo Designer applications for...
How do I unlock the SQL library in SoMachine v4.2?
Issue: How do I unlock SQL library in SoMachine? Product Line: SoMachine Resolution: Please see attached SQL license activation and installation document...
What causes Concept error message "11109 Bad rule-dialogue variable identifier"?
This error usually occurs when importing a project with the Concept Converter. Go back to the version of Concept from which the project was converted....
Could not initialize CoDeSys minimal package error
Issue: Getting a message in SoMachine "Could not initialize CoDeSys minimal package" Product Line: SoMachine all versions Resolution: You need to...
I already have a serial number for Schneider Electric Automation and HMI programming software, where can I download it?
Issue Customer has all of the information that is needed for a software installation except for the media itself. Product line Unity Pro, ProWORX...
In SoMachine, how do I extract a bit from a word
Issue: How to extract a bit from a word in SoMachine? Product Line: SoMachine Environment: SoMachine Resolution: Please use function block WORD_AS_BIT
Results 1 - 10 of 100