Technical FAQs

Ask a Question

Filter results

Clear
What is the Modbus TCP/ IP option for a ATV660 ?
Issue:  What is the Modbus TCP/ IP option for a ATV660 ? Product Line: ALTIVAR PROCESS SYSTEM Environment: All   Cause: Product Selection & Services...
What communication options (network protocols) are supported by the ATV312?
Issue:  What are the communication protocol that are available on the ATV312? Product line:   Altivar 312 Environment:   All range  All serial number   ...
What do the LED's indicate on the ATV58 Devicenet card?
Issue: What do the LED's indicate on the ATV58 Devicenet card?   Product Line: ATV58   Environment: All models and serial numbers with VW3A58309U...
Can the TSXETG100 gateway operate in modbus slave mode to connect a display unit in modbus master mode?
Yes, the TSXETG100 gateway is configured in Modbus master mode by default, but it can also be configured in Modbus slave mode. It can therefore be...
How can I position the switches of a TSXPACC01 box?
Follow the instructions in the diagram below:
What is FactoryCast?
The term Factory Cast refers to our Web enabled systems There are three types: FactoryCast - PLC processors in the TSX Micro, Premium and Quantum...
What is the pin-out of the RJ45 socket of an ATV31 / 312 for connection of Modbus, CanOpen and PowerSuite cables
     The RJ45 socket of the ATV31/312 can be used for connection to the following networks and accessories:      a PLC via a Modbus bus or via a CANopen...
Which network Protocols are supported on the Modicon STB distributed I/O?
The following network interface modules are avilable for the Modicon STB distributed I/O system Ethernet Modbus TCP/IP STB NIP 2311 dual port Standard...
Is TwidoSuite or Twido Soft software compatible with Windows 7?
Twido Soft software will never be compatible with Windows 7 as this software is obsolete. However, TwidoSuite version 2.31.4 is compatible with Windows...
Can I reset the IP address of an Ethernet Advantys STBNIP2212 if the IP address is not known?
If the IP address of an STBNIP2212 is not known, there are several options available. 1. MAC based default IP address To access the module via its...
Results 1 - 10 of 64