Technical FAQs

Ask a Question

Filter results

Clear
Preventa XY2C_How to order the commercial reference XY2CH13150H7 in 2019? is it available to order?
Please note that the XY2CH13150H7 commercial reference is available to order in 2019, under internal logistic reference XY2CH13150H7AC. Please contact...
How can I tell if my ATV61 or ATV71 drive is in sleep mode? (Low speed timeout active).
Issue: How can I tell if my ATV61 or ATV71 drive is in sleep mode? (Low speed timeout active). Product Line: ATV61 / ATV71 series drives. Environment:...
8839 EFD... is an invalid part #. Also 8839 MFD... 8839 SFD... 8638 48U... 8639 48U... 8639 22U...8839 CPD... 8930 IFD... SFD212...
Issue:  The part number does not come up as a good part number in Q2C. Product Line:   EFlex, MFlex, SFlex with non-standard Mods, Enclosed Drives,...
Are there any specific lifting drawings for Ringmaster
Drawings detailing the lifting arrangements are available on request. Lifting lugs are fitted to all units prior to despatch and general lifting and...
Is there a lifting drawing for GenieEvo
Drawings detailing the lifting arrangements are available on request. Lifting lugs are fitted to all units prior to despatch and general lifting and...
How can I order other sets of keys for the 30 mm dia. selector switches of the Harmony 9001 range?
Harmony 9001 range selector switches, part numbers: 9001KS11KxR 9001KS43K5R 9001KS53K5R can only be ordered with the following keys: Ronis No.455...
I have been quoted a long delivery time on a replacement XVC (monolithic) tower beacon, how can I obtain a replacement quickly?
The XVC (monolithic) tower beacons are not stocked by all UK Schneider Electric distributors. Those that do not stock the item will quote the extended lead...
INFORMATION BULLETIN - Using Global Outlet Groups simultaneously between AP79XX and AP8XXX series Rack PDUs with the same multicast IP range causes AP79XX PDU not to boot properly
Issue An issue has been identified with AP79XX series Switched Rack PDU users who enable the global outlet group functionality. If the user has AP79XX...
Results 1 - 8 of 8
  • 1