Technical FAQs

Ask a Question

Is it possible to compare or convert configurations from ATV61/71 to ATV6xx in SoMove?
Issue:   Can you compare or convert configurations from ATV61/71 to ATV6xx in SoMove? Product Line: Altivar 61, Altivar 71 , Altivar 630, Altivar...
Can I convert an XBTL1000 application (XBTF terminal) to Vijeo Designer (XBTGT/GK terminal)?
We have a Services & Projects offer making it easy to migrate XBTL 1000 applications created on XBTF terminals to Vijeo Designer applications for...
On a Magelis XBTGT display unit equipped with a USB port, how can I install a Runtime version that is earlier than the Vijeo Designer
Symptom: In Vijeo Designer, if you try to load an earlier Runtime version onto an XBTGT, the following message is displayed: "You are trying to transfer...
Is the ATV630 process drive compatible with the Multiloader tool?
Issue: Is the ATV630 process drive compatible with the Multiloader tool? Product Line: Altivar Process, ATV630 Environment: All Cause: N/A Resolution:...
Is the HMIGTU 12' display (HMIDT643) with built in WIFI compatible with both HMIG3U and HMIG5U?
Issue: It is not possible to select the HMIDT643 with built in Wifi for a HMIG3U in Vijeo Designer or Vijeo XD. Product Line: HMIG3U, HMIG5U, HMIDT643...
Will the B882-239 High Speed Counter support a quadrature input ?
No, the B882-239 does not support quadrature mode. You would have to use the B883-001 HSC for a quadrature operation. Legacy KB System (APS) Data:...
What is the minimum screen resolution to be used with Concept 2.6?
The minimum screen display resolution for Concept 2.6 is 800 x 600 pixels. 
Why is the 140CPS12420 not compatible with the 140CPS12400 when used in a redundant configuration ?
The two power supplies cannot share the output current  due to the difference in their internal design. The power supplies use different APS_SENSORS...
ION7300 series meter - kWh reading resetting to 0 after reaching 10,000,000
Regarding the Energy Rollout settings, the default value for the ION7350 is 10,000,000 but this value can be increased anytime using ION Setup, just...
Can the old withdrawable M type breaker be replaced by the new NW drawout breakers?
The withdrawable NW breakers can be retro fitted into the old Masterpact M chassis. However this is only available via the Service Department please...
Results 1 - 10 of 100