Browse FAQs

EcoStruxure Machine Expert v1.1 Installer returns message: Srcsdk.dll failed to register

Published date: 12 August 2019

Issue
When I install EcoStruxure Machine Expert v1.1, at 100%, I get a message indicating the message
Error 1904.Module C:\Program Files (x86)\Common Files\Schneider Electric Shared\SRCSDK\Srcsdk.dll failed to register. HRESULT -2147024770. Contact your support personnel.

Product line
EcoStruxure Machine Expert v1.1

Environment
Windows 8, Windows 10

Resolution
Click the Ignore button.
The installation will complete and you should still be able to launch Machine Expert afterwards.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.