Browse FAQs

What is the latest version of SoMachine Motion?

Published date: 12 August 2019

Issue
Is there a version of SoMachine Motion newer than v4.4.1? If so, what is the latest version?

Product Line
SoMachine Motion, EcoStruxure Machine Expert

Environment
PLC/PAC Configuration Software for Windows

Resolution
SoMachine Motion v4.4.1 is the last version of SoMachine Motion.
SoMachine Motion v4.4.1 and SoMachine v4.3 devices have now been integrated into the single configuration software tool called EcoStruxure Machine Expert.
The current version is EcoStruxure Machine Expert v1.1.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.