Browse FAQs

What is the speed regulation / accuracy of the ATV930 drive?

Published date: 02 August 2019

Issue:   
Needs the speed regulation or accuracy of the ATV930 drive with and without encoder
Product Line:   
ATV930
Environment:  
All with or without encoder
Cause:   
Speed regulation , accuracy
Resolution:   
ATV930:
- Open loop
Speed range: 1:500
Speed accuracy: 6% of nominal slip
​​​​​​​Torque accuracy: 10%
- Close loop
Speed range: 1:1500
Speed accuracy: 0.005% of nominal slip
​​​​​​​Torque accuracy: 5%
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.