Browse FAQs

Can the RM35JA31MW monitor positive and negative currents?

Published date: 30 July 2019

Issue:
Application is monitoring -4 to -20mA. 

Product line:
Zelio Control and Measurement

Environment:
RM35JA31MW

Cause:
Documentation shows on 4-20mA does not clarify postive or negative.

Resolution:
Yes, the RM35JA31MW can monitor +4 to +20mA or -4 to -20mA.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.