Browse FAQs

What is the pickup voltage for the RSB series relays?

Published date: 30 July 2019

Issue:
Voltage at which the coil will engage

Product line:
Zelio Plug in Relays

Environment:
all

Cause:
Documents show drop out voltage not pick up voltage

Resolution:
The pickup up voltage is within 70% of the rated coil voltage. 

So for example on RSB1A120ED with a 48VDC coil, the pick up voltage is 33.6VDC.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.