Browse FAQs

Is it possible to upgrade firmware for PMEGPS0100 module by Unity Loader

Published date: 29 July 2019

Issue: Customer receives a new module and wants to upgrade the FW of the module

Product: Partner Module PMEGPS0100

Environment: Control Expert V14, Windows 10 Professional

Resolution:  The PMEGPS0100 does not currently support  firmware updates using Unity Loader. The PMEGPS0100 supports web based firmware updates while in Boot Loader mode. To enter the boot loader, insert a paper clip or other small device through the small hole in the front panel labeled “Setup”. Depress the switch behind the hole until the front panel LEDs start to flash, approximately 5 seconds.
While accessing the webpage, the correct file can be browsed and downloaded to the GPS module.





 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.