Browse FAQs

What are the HMIPCCU27 Certifications?

Published date: 26 July 2019

Issue
What are the certifications for the HMIPCCU27?

Product Line
Magelis Modular Box PC

Environment
Physical HMI

Resolution
The Certifications for the Box iPC HMIPCCU27 is as follows:
- Industrial Control Equipment (UL 61010-2-201 and CSA C22.2 N° 61010-2-201) and for use in Class I Division 2 hazardous (classified) locations (ANSI/ISA 12.12.01 and CSA22.2 N°213). Refer to product markings. 
- CCC, RCM, and EAC. Refer to product markings. 
- CE Atex and IEC Ex as 3GD equipment category (for DC models). Refer to product markings. 
- CE Atex and IEC Ex as 3D equipment category (for AC models). Refer to product markings.

For more documentation on each certification, please see the "Box PC" column of this link:
http://static.schneider-electric.us/assets/1-product-offers/12-Magelis_HMI_iPC_Certification_Links.htm
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.