Browse FAQs

If I have an older Magelis HMISTU855, can I purchase a new HMIS85 screen to replace the original screen?

Published date: 26 July 2019

Issue
Older Magelis HMISTU855 and HMISTU655 are not compatible with new HMIS65 and HMIS85 screens, respectively.
For Magelis HMISTU855 and HMISTU655, what year are they compatible with new replacement screens?

Product Line
Magelis HMISTU

Environment
Physical Touchscreen HMI

Resolution
Magelis HMISTU855 and HMISTU655 series had a sourced component change in 2012 (upgraded ROM from 16MB to 32MB) which meant that the HMISx5 screens manufactured later than 2012 would not be compatible on HMISTU back modules manufactured before this change.

Therefore, HMISTU series back modules with dates of manufacture 2013 or newer will be compatible with HMIS65 and HMIS85 screens purchased now. Anything older would require replacement of both the screen and back module.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.