Browse FAQs

Magelis shows error "configuration file is not unicode"

Published date: 19 July 2019

Issue:
The Magelis HMI fails to boot properly and there is an application halt. The error on the dialog states the following:

Config problem:the configuration file is not unicode          
KAOScore:PortableProjectConfiguration.cpp:line 406


Product Line:
Magelis HMI programmed Vijeo Designer (any version)

Resolution:
This error is a result of a corrupt Vijeo Designer installation on the PC where the software is installed. To resolve this issue, please re-install Vijeo Designer and re-download to the HMI.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.