Browse FAQs

What is the part number for an auxiliary contact for 2510F?

Published date: 05 August 2019

Issue:
2510F/K auxiliary contact

Product Line:
Manual Starters and Switches

Environment:
Class 2510 Type F, Type K

Resolution:
2510F and 2510K manual starters do not have an auxiliary contact available. The 2510M or GV2 devices are available with the option to add an auxiliary contact.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.