Browse FAQs

How many built-in RJ45 communication ports in ATV630 drive?

Published date: 23 July 2019

Issue:
How many built-in RJ45 communication ports in ATV630 drive?

Product Line:
ATV630

Environment:
All serial numbers

Cause:
Customer wanted to know how many serial ports comes with the ATV630 drive.

Resolution:
The ATV630 has 2 built-in RJ45 communication ports as standard:
1 Ethernet Port (TCP only)
1 Modbus Serial Port
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.