Browse FAQs

How can I set up VIA (0-10V) speed reference on the ATV212 with 70Hz as max speed?

Published date: 25 July 2019

Issue:
Wants to use 0-10VDC on VIA scaled at 0-70Hz

Product Line:
ATV212

Environment:
All serial numbers

Cause:
Customer wanted to set 70Hz as max frequency using VIA (0-10V).

Resolution:
In order for drive to run up to 70Hz using VIA (0-10V) signal, drive needs to be programmed as follow:
FNOD=1
FH=70
UL=70
F201=0
F202=0
F203=100
F204=70


 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.