Browse FAQs

Is it possible to embed an image source file in a VDZ file?

Published date: 26 July 2019

Issue:
Vijeo Designer cannot find the image source files for the application if it is opened on another PC that does not have the same source files saved at the original location as specified.

Product Line:
Vijeo Designer (all versions)

Resolution:
It is not possible for the VDZ file to of Vijeo Designer to include the Image source files at some location (ex. X:\ Some Folder) on the PC when Vijeo Designer exports the file.
We suggest to zip the images folder and send it along with the project file or store the file in a Toolchest folder and export that to save it.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.