Browse FAQs

What's third party gateway can be added to use with Lonworks on the ATV630 or ATV930 drives?

Published date: 25 July 2019

Issues:
What's third party gateway can be added to use with Lonworks on the ATV630 or ATV930 drives?

Product Line:
Altivar ATV630 ATV930

Environment:
All model numbers, all serial numbers

Cause:
Customer would like to know if he can use Lonworks on the ATV630 drive. 

Resolution:
If you need to use Lonworks on the ATV630 and ATV930 drives, then you need to add a third party gateway such as Anybus communicator.  See link below for more information on Anybus communicator - Lonworks.

https://www.anybus.com/products/gateway-index/anybus-communicator/detail/anybus-communicator---lonworks

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.