Browse FAQs

PM8000 series firmware version 2.1.0 and release notes

Published date: 29 July 2019

Issue
PM8000 series firmware version 2.1.0 and release notes

Product Line
PM8000 series meter

Environment
PM8000 series firmware

Cause
A user would like to upgrade the firmware on a PM8000 series meter to V002.001.000

Resolution
*Warning: The firmware utilities listed here can cause permanent damage to your product if applied incorrectly. Before downloading any firmware updates, verify the firmware you are downloading is appropriate for the specific model number of your product. If you have any doubts, contact Technical Support for guidance.*

*Warning: Devices should be disconnected from all monitoring software before performing a firmware upgrade*


Release Notes: PM8000 firmware to address new and updated features for firmware version 2.1.0

For PM8000 V002.001.000 Firmware and Associated Files: 'PM8000 v 2.1.0 firmware'

Updates: This version implements the new features Enhanced firmware upgrades, PTP time synchronization, Secure webserver (HTTPS), and other.

Please see the following link for more information regarding 'What's new in PM8000 series meter firmware v2.1.0'

Notes: This firmware update is intended for PowerLogic PM8000 meters. ION Setup 3.1 or later must be used.

Please downloaded ION Setup 3.1 before upgrading the PM8000 to firmware v2.1.0 'ION Setup Latest Release'

For instructions on upgrading the firmware using ION Setup, please follow knowledge base article FA244316

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.