Browse FAQs

What is the life expectancy for ABL8 Power Supply?

Published date: 01 August 2019

Issue:
ABL8 Life Cycle

Product Line:
Power Supplies

Environment:
ABL8, ABL7, ABL1

Resolution:
Unlike a typical electromechanical device, there are several variables that will directly impact the life expectancy of a solid-state device in a given application.
The ambient temperature is a determining factors which may limit the power that an electronic power supply can deliver continuously.
Excessively high temperatures around the electronic components significantly reduce their life.
Environmental conditions, such as humidity and dust may also affect operation and life cycle. 

Since device does not have moving mechanical parts, a specifi life cycle does not apply. 
Schneider has tested an estimated MTBF, see the specification attached.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.