Browse FAQs

Can I save an offline configuration for the EM4800 using the EM4800 Configuration Tool

Published date: 29 July 2019

Issue:
End user would like to save a configuration file for the EM4800 while not being connected to the EM4800.

Product Line:
EM480

Environment:
Meter Configuration Software

Cause:
End user may not have the EM4800 meter present and would like to use the configuration software

Resolution:
The EM4800 Configuration Tool must be connected to an EM4800 over ethernet in order to be used. If you do not have an ethernet connection to the EM4800 meter you may get an error message that looks like the picture below




The error will be cause by either not inputting an IP address in the IP field or that the IP address you have entered is correct. 

If you need more information or the install file for the EM4800 configuration check out FA212442
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.