Browse FAQs

S-Flex 212 BACnet card. Is the transceiver fail-safe, non fail-safe?

Published date: 23 July 2019

Issue:
Has a ATV212 in a S-Flex, with a BACnet card. Wondering if the transceiver is fail-safe, or not?

Product line:
ATV212, Altivar 212

Environment:
all

Cause:
Customer asked about S-Flex 212 BACnet card. Is the transceiver fail-safe, non fail-safe?

Resolution:
Transceiver Type
- RS485 Transceiver is Fail Safe on ATV212.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.