Browse FAQs

Why doesn't my Vijeo Designer project with a Panasonic FP series driver build?

Published date: 26 July 2019

Issue:
When Vijeo Designer is installed with SoMachine, it is not possible to use the Panasonice FP series SIO driver. The upgrade code cannot be entered in SoMachine's copy of Vijeo Designer.

Product Line:
Vijeo Designer installed with SoMachine (all versions)

Resolution:
The solution is to uninstall the Vijeo Designer installed with SoMachine and re-install Standalone Vijeo Designer with an appropriate license.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.