Browse FAQs

How do you mount the TeSys D Contactor with Everlink Terminals in to a panel with screws or bolts?

Published date: 01 August 2019

The TeSys D contactors fitted with the Everlink Terminal strip can be mounted in a panel with M4 screws or bolts

Please watch the video below on how to prepare the contactor for mounting



The TeSys Range of contactors this applies to:
LC1D40A**
LC1D50A**
LC1D65A**

Fixings up to 6.5mm diameter can be used or M4 screws are recommended
The hole centers for the panel are:
TeSys D Contactors with Everlink Terminals Mounting centres

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.