Browse FAQs

What does a P or H symbolize in an ATV12 drive part number?

Published date: 05 July 2019

Issue:
What does a P or H symbolize in an ATV12 drive part number?

Product Line:
Altivar 12

Environment:
All

Cause:
Part number

Resolution:
The ATV12 drives are available as H or P version.  Part numbers with H are drives with a standard heatsink on the back of the drive.  
Ex: ATV12H037M2 has a heatsink.  Replace the H with P for drives without a heatsink.  Instead of a heatsink, these drives have a smooth, flat metal back that can be mounted to a thermally conductive machine surface.  
The P version is available up to 1HP for single phase input voltage and up 5HP for three phase input voltage. 

H version:     P version:        

Refer to Installation Manual BBV28587 for further details: https://www.schneider-electric.com/en/download/document/BBV28587/
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.