Technical FAQs

Ask a Question

How do we make a switch that stays down when the bit is high?

In Vijeo Designer, we must make use of two objects to animate a switch that stays down while the bit is high and that is also able to reset the bit when touching it.

We make use of 
1) A radio button (to set the bit and to stay down when the bit is high)
2) An invisible switch to be used to reset the bit. The switch has a visiblity condition to only appear when the bit is high.

Please see attached example.
Was this helpful?
What can we do to improve the information ?