Technical FAQs

Ask a Question

How to save the active configuration in one of the 3 backup slots of the Webserver? Is all configuration data saved?

  • Yes, all data can be saved in one of the 3 backup memory slots of the HU250 memory.
  • The T300 configuration uploaded into the product or saved externally is a compressed tar.gz filetype. This file contains the complete equipment configuration, including SC150 settings and  system parameters (IP address, modem parameters, etc.). But it excludes SC150 IP addresses, user parameters and RBAC access rights which are stored into the rights management tool (SAT).
  • Please see the attached file for an excerpt from the T300 user manual for details. 
Was this helpful?
What can we do to improve the information ?