Browse FAQs

Where are the specifications located for the Embedded ATV340 Encoder?

Published date: 25 July 2019

Issue:
Where are the specifications located for the Embedded ATV340 Encoder?

Product Line:
ATV340, Altivar machine

Environment:
All

Cause:
NA

Resolution:
The Embedded Encoder specs for ATV340 Drives are located in the ATV340 Installation Manual.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.