Browse FAQs

What would cause the drives HMI to show RDY when the remote start on logic input is being given?

Published date: 26 July 2019

Issue:
Drive state stays at RDY when the remote start on logic input is being given

Product Line:
Altivar drives. 

Environment::
ATV12, ATV212, ATV312, ATV320, ATV61, ATV71, ATV630, ATV930 

Cause:
Drive will not run. 

Resolution:
a) Verify the run command at the drive terminals.
b) Measure voltage on the drive inputs to verify commands. 
c) Verify the drive programming is set for terminal command. 
d) Verify the drive programming for 2 wires or 3 wires control 
e) Verify the command channel and command switching 
f) Verify the drive is not in local mode control.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.