Technical FAQs

Ask a Question

PM55xx meters now supports Ethernet/IP communication protocol

Issue
Customer is asking if PM5500 meter supports Ethernet/IP

Product Line
PM5560 (METSEPM5560)
PM5563 (METSEPM5563)

Environment
Communication protocol support

Resolution
PM55xx meters does support EtherNet/IP communication protocol starting with Firmware 2.5.2 that was released on Feb 2018. Meters with older version of firmware need to be upgraded to version 2.5.2 to support Ethernet/IP protocol.

PM55xx Firmware Version 2.5.2 can be downloaded from here

EtherNet/IP features overview:
The CIP (Common Industrial Protocol) application layer defines a set of application objects and device profiles that define common interfaces and behaviors. In addition, CIP communication services enable end-to-end communication between devices on the different CIP networks. EtherNet/IP maps the CIP communication services to Ethernet and TCP/IP, enabling multi-vendor interoperability between devices on Ethernet as well as with the other CIP networks. 

EtherNet/IP defines two primary types of communications:
•    Cyclical Exchanges (Implicit Exchanges)
•    Messaging (Explicit Exchanges)

EtherNet/IP is enabled by default on firmware v2.5.2. This feature can be enabled/disabled by navigating to the EtherNet/IP settings available through the meter’s display under Maint > Setup > Comm, or via the relevant section in the meter’s web-page interface.

For more details on the EtherNet/IP features in PM5500 Series, please refer to the PM5500 Series User Guide version 05 or later.

More information:
You may find firmware, user manual, installation guides, and other documentation on the Schneider Electric Shopping Kiosk, or the Schneider Electric Web Site.
Was this helpful?
What can we do to improve the information ?