Technical FAQs

Ask a Question

Easy 9+ Flush mount kit Installation - Video




Installation of the flush mount kit, removing the lid of the chosen board (only applies to boards below) applying flush mount surround over the board and then placing the lid back in its position, then once in place you will need to secure the kit to the wall of the apllication you are installing the board.

Section of the flush mount kit is key explained below:
as per page 13 of the introducing Easy9+  product brochure.

EZ9EFLKIT12 = Compatible boards for these 12Way & 4+4 Way.
EZ9EFLKIT16 = Compatible boards for these 16way 6+6way 2+5+5way
EZ9EFLKIT20 = Compatible boards for these 20way 8+8way 2+7+7way

Flush mount trims drawings attached.

The board will recess 70mm when flush kit is applied this will leave 40mm for the lid to be shown on the wall.


 
Was this helpful?
What can we do to improve the information ?