Browse FAQs

How can you set up preset speeds on the ATV630 and ATV930 drives?

Published date: 10 July 2019

Issue:
How can you set up preset speeds on the ATV630 and ATV930 drives?

Product Line:
Altivar Process ATV600 ATV900

Environment:
All

Cause:
Setting up preset Speeds

Resolution
Complete Settings >Preset Speeds > 2 Preset Speeds = DIX, then go to  Preset Speed 2 = (desired frequency) 30hz or DIX  then go to  Preset Speed 4 and set up your 3rd and 4th speeds.. See the table below. 
The manual contains a truth table that explains which inputs need to be On/Off for multiple preset Speeds to work, see example attached.

https://www.schneider-electric.us/en/download/document/EAV64318/
 

Was this helpful?

What can we do to improve the information ?