Browse FAQs

Is there a blank NetShelter door badge available? If so, what size is available and how many are in the package? Can APC provide custom door badges?

Published date: 05 July 2019

Issue: 
Customers may want to have their logo on the cabinet. 

Product Line: 
NetShelter SX

Environment: 
All models, all serial numbers. 

Cause: 
Customers may not want the APC by Schneider Electric logo on their cabinets, or may want additional badges. 

Resolution: 

We offer sku AR7001X384, which is a pack of 40 blank door badges, The door badge is oval, and the dimensions are 71.5 mm wide x 39.4 mm high. 
To date we have not offered custom printed door badges attached to the cabinet. To process a request please contact your APC Sales Rep, or the CustomRacks team. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.