Search FAQs
What is the height of the Isobar three phase B board range of extension boxes.
The height of the Isobar B board extension boxes is 270mm.
Several extension boxes maybe stacked together if more space is required.
Some examples are below:
They can be mounted either top or bottom of the distribution boards.
Please refer to catalogue for additional information and other options.
Several extension boxes maybe stacked together if more space is required.
Some examples are below:
Part Reference | Description |
SEA9BNEXN | Plain front cover for additional wiring space |
SEA9BNEX034N | Mounting of DIN devices, overall door and cutout for 17 x 18mm poles |
SEA9BNEXA14N | Single phase add on distribution board 14 way |
They can be mounted either top or bottom of the distribution boards.
Please refer to catalogue for additional information and other options.
Released for:Schneider Electric UK
Explore more
Explore more