Technical FAQs

Ask a Question

What is the maximum Amperage for the Acti 9 iCT contactors?

The maximum Amperage for the Acti9 iCT contactors is 100A at In (AC7a).

This is only available in the following iCT Contactors
 
Poles AC7a Rating Control Voltage Part Number
2 100A 220..240Vac A9C20882
4 100A 220..240Vac A9C20884

Other iCT contactors are available, please refer to the Acti9 Ready to Install Catalogue
Was this helpful?
What can we do to improve the information ?