Browse FAQs

How to change the template on an ATV630 and ATV930 so that the 0 % speed is at low speed, instead of 0 hz?

Published date: 25 July 2019

Issue:
How can the customer change the template on an ATV630 and ATV930 so that they show 0 % speed is at low speed, instead of 0 hz?
 
Product Line:
ATV630 ATV930
 
Environment:
Pedestal and deadband
 
Cause:
n/a
 
Resolution:
Parameter BSP can have a setting of Standard, Pedestal, Deadband or Deadband 0 %.
When you see the Keypad: BSP can be standard , Deadband, pedestal or pedestal at 0%.
The term is inverted on keypad.  Deadband should be Pedestal and pededstal /pedestal at 0% should Deadband/Deadband at 0%. 
Same problem with SoMove: 
The solution to set Pedestal like on ATV71, is to set Deadband on ATV6XX/ATV9XX. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.