Browse FAQs

Can you convert settings from an ATV32 or ATV312 program into an ATV320 using SoMove Software?

Published date: 14 August 2019

Issue: 
Can you convert settings from an ATV32 or ATV312 program into an ATV320 using SoMove Software?
 
Product Line:
ATV32, ATV320, ATV312
 
Environment:
All models, all serial numbers
 
Cause:
N/A
 
Resolution:
Yes
  1. Open Somove and from the Home Screen click on [Device Conversion] button on the left under tools
  2. Choose your source ATV32 or ATV312 file that you want to convert.
  3. Choose your target location (ATV32 to ATV320) or (ATV312 to ATV320)
  4. Change target DTM to ATV320
  5. Choose Convert
  6. Choose if you want the B suffix or the C suffix version ATV320 drive. 
  7. Option window comes up to allow you to save changes to txt file.  
  8. Skip saving the changes and continue 
  9. Now your new ATV320 file comes up, and you can save this new file to your PC
  10. File menu choose Save as enter and name your new file to save. 




 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.