Browse FAQs

Can the ATV320 be programmed without power?

Published date: 26 July 2019

Issue:
Can programming be done on the ATV320 Drive without Line Voltage?
 
Product Line:
ATV320, Altivar 320
 
Environment:
All
 
Cause: 
Customer wants to program the ATV320 with a Multiloader without line or control voltage connected to the drive.
 
Resolution:
Yes, the ATV320 can be programmed via the Multiloader with no external power source applied.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.