Browse FAQs

What is the Fan PID function on the Altivar 600 Process Drive?

Published date: 22 July 2019

Issue:
What is the Fan PID function on the Altivar 600 Process Drive?

Product Line:
Altivar 600 Process Drive

Environment:
All products of Altivar 600 Process Drive

Cause:
N/A

Resolution:
The Fan PID allows the user to setup a basic PID function when the drive's Macro Configuration (Menu 7.1) is set to Generic Fan Control.
There is no difference in the parameters and the settings than when setting up a pump PID. 
To access go to [Fan] - [PID controller]

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.