Technical FAQs

Ask a Question

Why does my circuit breaker keep tripping when the blinds change direction?

When you shut off of a single phase motor followed by a quick change in direction, it can cause the motor to work harder because of the change of direction, causing the motor to consume a larger amount of current, in use of different terms it has a larger in rush current. The reason why it consumes a larger amount of current is because the motor is in the process of reversing its magnetic poles which is accomplished by reversing the polarity of the starter winding.
This may be enough current to trip some Circuit breakers. Failure to extend the change over time may result in the motor burning out or consistent nuisance tripping of a circuit breaker or potentially even the motor not reversing direction. By increasing the “change over delay” to meet the blind manufacturers specifications should prevent any of these issues from happening.
Was this helpful?
What can we do to improve the information ?