Browse FAQs

Do the 3090TB4/3090TB6 shorting blocks include a cover?

Published date: 31 July 2019

Issue
Customer wants to know if shorting blocks with part number 3090TB4 or 3090TB6 include a cover. 

Environment 
Wiring, installation

Cause 
MySchneider, Digest and the cut sheet for the shorting blocks do not specify if a cover is included.  

Resolution
The 3090TB4 and the 3090TB6 do not include a cover.

Note: These were part numbers for shorting blocks that included a cover,
they are now Obsolete

37GP1704SC - 4 pole shorting block w/ cover
37GP1706SC - 6 pole shorting block w/ cover
37GP1708SC - 8 pole shorting block w/ cover


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.