Browse FAQs

Can the ATV320 be used for single phase input to run a three phase motor?

Published date: 09 August 2019

Issue:
ATV320 single phase supply to a three phase motor

Product Line:
ATV320, Altivar 320 Machine drive

Environment:
All models

Cause:
Short circuit and HP ratings for VFDs supplied with single phase power.

Resolution:
Yes, the ATV320 is suitable for single phase supply to three phase motors.  See the information included in the Getting Started Annex, document NVE21777 attached to select. 

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.